2024-05-15 9:16 AM - last edited on 2024-06-11 7:33 AM by Amel NASRI
What is the difference between ST-LINK/V2-1 and V2? Where can I buy v2-1?
Or are you buying v2 and updating the firmware?
2024-05-15 9:27 AM
The V2-1 variant is the one used on NUCLEO / DISCO / EVAL boards, it provides for the VCP and MSC, and support for mbed. ie comes with a COM port for UART connectivity and drag-n-drop on binary firmware.
You can't just update the firmware, as a different more powerful STM32F103 was used, and where are those pins/functionality going to come out?
New, you'd want to be looking at getting an ST-LINK/V3 model
2024-05-15 9:31 AM
Keep in mind that ST-LINK/V3 only works with STM32 parts.
2024-05-15 9:34 AM
ST-LINK/V2-1 is onboard on (many) STM boards (nucleo, disco..); V2 is the separate debug probe.
ST-LINK/V2-1 has VCP and "Virtual Disk" to flash a file , V2 has not.
(You cannot change V2 -> V2-1 by update.)
ST-LINK/V3 (mods, miniE ) has it also and is faster (hi-speed USB), so this is the actual "right" one .
2024-05-15 9:39 AM
Not sure that was the question asked, but Segger J-Link and CMSIS-DAP would be more general alternatives.
2024-05-16 8:04 AM
So could I use the microB to USB cable like when I used the Nucleo board?
2024-05-16 9:31 AM
For..what ?
+ Which nucleo ?
We’re moving the ST Community to a new platform to give you a better and more reliable community experience.