STM32 MCUs Boards and hardware tools

Ask questions and find answers on STM32 hardware set-ups, including schematic-related challenges, debugging probes, power configurations, and more.

cancel
Showing results for 
Search instead for 
Did you mean: 

Forum Posts

Resolved! STM32F429I-DISCO1 Firmware and IDE's

Hi, I have an STM32F429I-DISCO1 board. I have been learning how to use it and I thought it would be good to see how the professionals do it by looking at the original firmware. I downloaded en.stsw-stm32138, which has STM32F429I-Discovery_FW-V1.0.3 i...

Lanceh by Associate III
  • 1760 Views
  • 2 replies
  • 0 kudos

STM32 Nucleo support for 1.8V

Hi I'm using the STM32H755ZI board which has the option for 1.8V DVDD (using JP5). Does switching DVDD to 1.8V from 3.3V limit the functionality of the board in any way ? Are the interfaces (CAN, I2C, SPI, UART etc) still functional at 1.8V ?  Thank...

smul by Associate
  • 1194 Views
  • 1 replies
  • 0 kudos

STM32G031K8 Nucleo Error in RAM

HiWe've got here 3 STM32G031K8 Nucleo. 2 of them had problems with RAM access. 1 works fine at the moment.For example STM32CubeProgrammer shows by RAM DumpKeil shows STLink Utilities hangs by Access of some RAM address. Is this a known Problem?Is the...

Prog.png keil.png
CanRF by Associate III
  • 1579 Views
  • 2 replies
  • 0 kudos
Announcement

We’re moving the ST Community to a new platform to give you a better and more reliable community experience.