2024-06-21 6:00 AM - last edited on 2024-06-21 6:20 AM by Amel NASRI
Hi
I'm using the STM32H755ZI board which has the option for 1.8V DVDD (using JP5).
Does switching DVDD to 1.8V from 3.3V limit the functionality of the board in any way ?
Are the interfaces (CAN, I2C, SPI, UART etc) still functional at 1.8V ?
Thanks in advance for any help
2024-06-22 7:56 AM
Have a loo at the datasheet
5.3
Operating conditions
5.3.1
General operating conditions
E,g,USB needs 3 V minumum
We’re moving the ST Community to a new platform to give you a better and more reliable community experience.