STM32 MCUs Boards and hardware tools

Ask questions and find answers on STM32 hardware set-ups, including schematic-related challenges, debugging probes, power configurations, and more.

cancel
Showing results for 
Search instead for 
Did you mean: 

Forum Posts

Nucleo-G0B1RE I2C2 Communication

I am using the Nucleo-G0B1RE board for I2C communication with BMS AFE IC. I am able to communicate with AFE if i use I2C1 port. I have tested it with [PB9, PB8] and [PA9, PA10]. If i use I2C2 or I2C3 it doesn't work. In case of I2C2 it only works if ...

Connection issue with B-L462E-CELL1

Hello,After purchased a  B-L462E-CELL1 and find ICCID and active on Truphone....below is my tera term output *********** CST_network_status_test_mngt ********ATParser:*** SEND (size=10) ***AT+CEREG?<CR><CR><LF>+CEREG: 2,3<CR><LF>ATCModem:NetworkState...

Mayank2 by Associate II
  • 3558 Views
  • 5 replies
  • 0 kudos
Announcement

We’re moving the ST Community to a new platform to give you a better and more reliable community experience.