2025-01-19 8:16 AM
Hello,
I have a brand new STM32C0116-DK evaluation board (official) and I fear I just bricked the on-board ST-Link :\
I wanted to run an example (blink LED) from the CubeIDE provided examples. When I pressed run, a popup displayed to notify me the ST-Link firmware should be updated. So I launched the process but the popup window freezed. I closed CubeIDE and disconnected the USB cable... Now the ST-Link LED is blinking RED at about 0,5 Hz and Windows doesn't detect any USB device at all (nothing is enumerated in device manager, nor a "USB device not working properly" popup) I think I did a mistake...
I will need it to work from home home for the two weeks. Is there a way I can force it to pass in update mode? I only have this board at hand right now, so is the only ST-Link debugger I have (had)...
Solved! Go to Solution.
2025-01-19 11:38 AM
Its not so easy to brick the board...
STM32CubeProgrammer is IMHO the most reliable tool for accessing a board including ST-LINK updates.
> ST-Link LED is blinking RED at about 0,5 Hz
This happens when power is on, but no USB comm. Try to reset the USB port / repower the computer.
hth
KnarfB
2025-01-19 11:38 AM
Its not so easy to brick the board...
STM32CubeProgrammer is IMHO the most reliable tool for accessing a board including ST-LINK updates.
> ST-Link LED is blinking RED at about 0,5 Hz
This happens when power is on, but no USB comm. Try to reset the USB port / repower the computer.
hth
KnarfB
2025-01-20 9:47 AM
[Resolved]
Hi KnarfB,
Thank you for your quick answer! Yes I know ST products are robust, but wasn't sure at which point the firmware was secured!
This morning the board was working fine after a complete PC shutdown and USB unplugged. I think it was an issue with the computer USB 3.2 port. When I restarted the computer this morning, I plugged the board on a USB 2.0 port and it was working fine. I did not try again the USB 3.2 port at the moment but I was able to work with the board.
In the same time I ordered a second kit regarding as cheap as it is ;)
We’re moving the ST Community to a new platform to give you a better and more reliable community experience.