Resolved! NUCLEO-C5A3ZG STM32C5 QSPI Display Bring up Project
This project tests the STM32C5's XSPI capability to drive QSPI display using the NUCLEO-C5A3ZG M.2/SerialMem connector. GitHub - stm32-hotspot/STM32C5-M2-Serial-Mem-QSPI-Display · GitHub
Ask questions and find answers on STM32 hardware set-ups, including schematic-related challenges, debugging probes, power configurations, and more.
This project tests the STM32C5's XSPI capability to drive QSPI display using the NUCLEO-C5A3ZG M.2/SerialMem connector. GitHub - stm32-hotspot/STM32C5-M2-Serial-Mem-QSPI-Display · GitHub
My hardware has the I2C pins (SDA and SCL) connected incorrectly, and I cannot change them because the hardware is already built. Is there any way I can fix this issue from the firmware side? Can I change the pins through software? hear attach my sch...
On the STDC connector, Pin 13/14 are virtual com port signals T_VCP_RX and _TX.Which one is input and output? They have cryptic comments like "Output for STLINK-V3SET" (for _RX) - Is RX an output and connects to the RX pin on the STM32? Or is it an i...
For product A (68-pin VFQFN package), pins 31 and 66 are VCAP pins, and 2.2uF capacitors have been placed on each pin. Should pins 33 and 66 be connected to each other, or is it sufficient to place the capacitors on each pin individually?
Hi,I am using stm32h745 dual core microcontroller. I want to bootloader application in this processor. The same process does not work with applications made with single core. Can anyone share a sample code for this? Or can you help me on how to apply...
Hi there!here i'm for ask another help. I use STM32G031 for write and read eeprom 24LC01B , and i work with where Address = 0x01;HAL_I2C_Mem_Write(hi2c, DevAddress, Address , I2C_MEMADD_SIZE_8BIT, &val, 1, 100);so if i wrote 7 byte everythingh work p...
I am designing interface board similar to MB1835 for our touchscreen to work with MB1829. STM32U5G9NJH6Q power supply VDD, VDDA, VDDIO and VDDUSB are all supplied with 1.8V. Thus, STM32U5G9NJH6Q GPIO is compatible with 1.8V signals. Touch Screen co...
Hello all,I would like to set SWCLK to permanent logic high, from pc side, in order to force bootloader loading in my custom board.Is that possible?Edit. Is any of the ST-link output signals (SWCLK/TCK, SWDIO/TMS, TDI) in strong logic high state by d...
The stlink port is not displayed in Device Manager or is not connected.
Hello , i have been getting this error very frequently across a few board 2x H7A3 and now i getting on H743 nucleo, sometimes i managed to resolve this by shorting boot0 pin and VCC pin then do a chip erase. Most of the time cannot resolve this err...
Hello,I hope you are doing great, I am facing the issue with NUCLEO-H743ZI2 Board, The LD6 is always ON and the IC U2 is getting overheated as soon as we connect the USB cable to dump the code and also unable to dump the code. It would be great if so...
We’re moving the ST Community to a new platform to give you a better and more reliable community experience.