2024-02-25 5:44 PM
Hi,
In AN3433, Appendix B says "The Tag detection calibration process must be performed when the application is initialized".
However in case that I don't use tag detector mode,
I don't have to process the Tag detection calibration, do it?
I want ST25R95's startup time to be as fast as possible.
Therefore I want to reduce the Tag detection calibration process.
Thanks
Solved! Go to Solution.
2024-02-26 12:13 AM
Hi,
the tag detector calibration is not needed if not using the tag detector feature. If the RFAL is being used in your application, you can set ST25R95_TAGDETECT_CALIBRATE to false in platform.h. This disables the call to st25r95CalibrateTagDetector() during initialization.
Rgds
BT
2024-02-26 12:13 AM
Hi,
the tag detector calibration is not needed if not using the tag detector feature. If the RFAL is being used in your application, you can set ST25R95_TAGDETECT_CALIBRATE to false in platform.h. This disables the call to st25r95CalibrateTagDetector() during initialization.
Rgds
BT
We’re moving the ST Community to a new platform to give you a better and more reliable community experience.