2018-10-31 12:23 PM
We are using VNQ5160 in a project, but those chips are now not avalible and we would replace them with VNQ5E160AK-E. Footprint and switching power is the same, the only main difference is in status pins, where older chip has status outputs and new has current sense.
As to documentation, current sense pins must not be left floating. Is this true also when CS_DIS is engaged?
Please find a schematics for the old project; can the same connection also be used with VNQ5E160?
2018-11-13 11:07 AM
Test is the best (when ST support fails and does not provide answer ...).
Works when Isense pins are left floating and Isense disable pin is pulled low.
We’re moving the ST Community to a new platform to give you a better and more reliable community experience.