2019-11-27 5:04 PM
I am repairing the power supply of AC-DC5V.
According to the VIPer22A data sheet, pins 5-8 are "DRAIN"
It was confirmed that the purchased VIPer22A has the same pin number 5-8.
However, the VIPer22A (4PY138) used for the AC-DC5V power circuit purchased separately does not have DRIN for pin 5 and pin 6.
Are there any devices on the VIPer22A where the 5th and 6th pins are not "DRAIN"?
If such VIPer22A is on sale, please let me know so I would like to buy it.
Please let us know the signal names of pins 5 and 6.
Please.
2019-12-02 5:01 PM
Add a question description.
Using a tester, we confirmed the connection between the pins.
as a result
Only the 7th and 8th pins are conductive. Pins 5 and 6 are not conducting. Therefore, the 5th and 6th pins are not considered “DRAIN�?.
Does "VIPer22A" have different pin assignment devices?
please answer.
We’re moving the ST Community to a new platform to give you a better and more reliable community experience.