2019-12-01 2:08 AM
Hi,
I'm using the VN340SP-E on a board to drive 4 output inductive loads from a 24V voltage
In one condition I connected solonoids (which are actually inductors) to the outputs.
I activated the 24V on the output stage and power was applied to the inductors, operating the solonids.
When I disconnected the power, with one inductor connected, the power went off and the DIAG signal stayed high
At another occasion, when I disconnected the power, with Two or more inductors connected, the power went off with the DIAG signal lowered for 5V or so, causing the device to be burned off and I can't use it anymore.
At one experiment a shift register, connected to the DIAG signal, burned off while the DIAG signall lowered.
Why does it happen? Can you help with this? How can I solve it?
Thanks,
Eldad
We’re moving the ST Community to a new platform to give you a better and more reliable community experience.