Power management

Discuss power management solutions. Ask questions and find answers on voltage configurations, short circuit protection, and programming.

cancel
Showing results for 
Search instead for 
Did you mean: 

Forum Posts

VN340SP-E DIAFG signal

Hi,I'm using the VN340SP-E on a board to drive 4 output inductive loads from a 24V voltageIn one condition I connected solonoids (which are actually inductors) to the outputs. I activated the 24V on the output stage and power was applied to the induc...

Should a inductor be added between Cin and the drain of MOS in the applicaion of Liner Voltage Regulator in L9779

 I've got a problem about the engine management IC——L9779. I would really appreciate that if you could help.Here is the thing:  A Liner Voltage Regulator has been built on this chip, which could transit the voltage from 12V to 5V and 3.3V.And this Re...

0690X000006CJQsQAO.png 0690X000006CJR2QAO.png 0690X000006CJR7QAO.png
Haigy Bob by Associate II
  • 2770 Views
  • 5 replies
  • 0 kudos

STEVAL SPIN3201 Hall Effect RPM Stability 3000RPM +/- 1.5RPM

Dear CommunityI have developed a BLDC motor drive with a senorles BACKEMF control using a DRV10983 IC.It uses sensor less control no halls used. If I look at the motors hall effects that are not used on the DRV10983 Chip My issue is that the speed is...

ST IHM08M1 Shottky Diode for Encoder and Hall

Hi,I need the circuitry on the IHM08M1 board for the encoder and hall sensors two times.I would like to ask, is there an alternative diode for the BATFILM30K, which is not built for SMD, instead built for THT.In the data sheet "Diodes and rectifiers"...

Initial torque problem in STSPIN32F0

I have tried to configure ​stspin32f0 as per the user guide instructions to get required starting torque from bldc ,it is not working properly.plese provide me the information what parameter i have to change to increase my starting torque.

Announcement

We’re moving the ST Community to a new platform to give you a better and more reliable community experience.