2023-01-02 4:27 AM
Hello ,
We want to drive two independent hub motor ( as like hoverboard) with STSPIN32G4 . Product overview says "Finally, with an additional external three-phase driver (such as the STDRIVE101) two independent 3-phase BLDC motors can be efficiently driven from the STSPIN32G4, offering an unprecedented BOM saving and application optimization." but I couldnt find any document .
Do you have any advice about that
Thank you
Abdullah KINIK
SAHA Robotik
2023-01-03 10:18 AM
Have you seen EVSPIN32G4, EVALSTDRIVE101?
hth
KnarfB
2023-01-03 12:18 PM
Hello,
Dual drive is doable with the STSPIN32G4, but this solution is not yet supported by the X-CUBE-MCSDK . If you plan to use the ST firmware solution, the dual drive is planned to be back with the summer release 2023 expected begining of July.
Regards
Cedric
We’re moving the ST Community to a new platform to give you a better and more reliable community experience.