2024-10-08 11:10 PM
Hello,
We are evaluating the STEVAL-STPM801 board, testing the STPM801 as integrated hot swap, soft start and oring protections device.
On the EVAL board the TM pins with nrs: 8, 13, 14, 27, 28, 29 are equipped with jumpers to select pull-up or pull-down, while in the datasheet of the STPM801 those pins must be connected to GND.
Also in the datasheet there is in chapter 5.1.5 STAND-BY mode enter/exit, in several graphs a pattern given for ENABLE-IN. I can not find the ENABLE pin.
However, on the EVAL board the signal connected to pin nr 8 in that figure 1 has the name TM_EN_1/2.
The TM lines are also feed to a jumper (e.g. JP17) with signal names like SPI1_*.
The difference between the Eval board and the datasheet makes it confusing.
Hope that anyone can clarify.
kind regards
2024-10-11 6:38 AM
Dear user,
Answering the questions:
Please let us know if you have other questions, we will be glad to reply to you.
Best Regards
2024-10-11 6:54 AM
Hello Fabiop,
See my feedback in italic:
regards
2024-10-11 7:19 AM
Dear user,
Q: Refering to figure 13, 14, etc: there is a pattern named "Enable pattern IN". On what pin this patterns must be supplied?
A: STBY_IN
Please let us know if you need something else.
Best Regards
We’re moving the ST Community to a new platform to give you a better and more reliable community experience.