2020-11-27 7:03 PM
This App Note is identified by the following meta-data:
Identifiers: AN4027, Doc ID 022604 Rev 1
Title: "12 V - 150 W resonant converter with synchronous rectification using the L6563H, L6699 and SRK2000"
Author: Claudio Spini.
Date: July 2012
Hello Sir/Madam,
Question 1: The schematic on page 12/38 shows a connection between D16K & R34. (Note: D16 anode is connected to L6699 pin 3, CF). That connection is marked "connection made by re-work". I seek an explanation as to why this connection was done.
Question 2: Several components on the schematic are marked "N.M.", eg: D16, C43. What does "N.M." mean?
Many thanks!
Edit 02-Dec-2020: Added image below, the relevant portion of the schematic.
Solved! Go to Solution.
2021-04-22 1:13 AM
Update 26-Apr-2021: This comment has been deleted, as it has been posted as a new question here:
https://community.st.com/s/question/0D53W00000jlWV8SAM/l6599at-gate-drive-pulses-appear-unexpectedly
Regards,
-F.Barone.
2021-04-22 6:49 AM
Hi @FBaro.1 ,
please open a new topic in the Power Management section
As above mentioned I am not in charge of resonant controllers, but if you post in the right place some others Community members can help you.
Have a nice day.
2021-04-22 4:14 PM
Hi @Cristiana SCARAMEL ,
thanks for your reply, as per your advice I have posted a new topic in the Power Management, here is the link:
Regards,
Fabio Barone.
We’re moving the ST Community to a new platform to give you a better and more reliable community experience.