Resolved! STSPIN250 EN/FAULT pin problem
good afternoon!I can’t read the FAULT state when the specified load limit is exceeded. the oscilloscope shows that the signal does not drop to a logical zero.my board
Discuss power management solutions. Ask questions and find answers on voltage configurations, short circuit protection, and programming.
good afternoon!I can’t read the FAULT state when the specified load limit is exceeded. the oscilloscope shows that the signal does not drop to a logical zero.my board
Hi, We notice that in Shutdown mode STEVAL-STWINKT1B + STEVAL-STMODLTE is consuming more power[36mA] than specified. But if we us only STEVAL-STWINKT1B than the current consumption is in nA, that's great but not when we plugin STEVAL-STMODLTE, it sh...
Hi, started using chip STC3115 in custom designed PCB. Everything is work fine, voltage and current measure good. But If I charging the battery SOC doesnt show correctly. I using it with driver from official STM site. I connected to chip 12500mA Li-p...
I'm seeing shoot through on the coil drives for the STSPIN32F0A custom implementation in the attached schematic. The attached scope shot has these channels:CH1: 24VCH2: CoilCH3: Low Side GateCH4: High Side GateYou can see the 700ns of deadtime when t...
Hi,we ar designing a Tupe C Power Delivery and Communication on a single USB type C port. SO, if we are not connecting any device to the USB port , then the communication circuitry must be off and should not consume any power. and when the source is ...
I'd like to porting software from P-NUCLEO-IHM03 (NUCLEO-G431RB + X-NUCLEO-IHM16M1) to NUCLEO-G474RE+ X-NUCLEO-IHM16M1. Are there hardware differences between NUCLEO-G431RB and NUCLEO-G474RE that exclude such software porting?I installed on my PC sof...
We’re moving the ST Community to a new platform to give you a better and more reliable community experience.