cancel
Showing results for 
Search instead for 
Did you mean: 

STMWB05N: SMP/Pairing Request does not trigger.

rsatina
Associate

Hello,

I am using STM32H735 and installed a Bluetooth module STM32WB05N.

For the STM32WB05N, it is configured as a transparent mode running as HOST + CONTROLLER firmware.  I got the firmware from this github: STM32WB05N Firmware.

I have modified STM32WB05N firmware to use the correct PINS and adjusted the baudrate to work with our MCU STM32H735.

So from STM32H735, I have successfully sent the ACI & HCI commands and is able to advertise my device.  I am using my Laptop to try and pair it using the windows bluetooth built in app and when I tried to pair my device, I got a confirmation from my STM32H735 and received the following events

  • HCI_LE_ENHANCED_CONNECTION_COMPLETE_EVENT

  • HCI_LE_ADVERTISING_SET_TERMINATED_EVENT

  • HCI_LE_CHANNEL_SELECTION_ALGORITHM_EVENT

After that the windows pairing failed.  I was expecting to receive more events and vendor events like:

  • HCI_LE_DATA_LENGTH_CHANGE_EVENT

  • ACI_ATT_EXCHANGE_MTU_RESP_EVENT

  • ACI_GATT_SRV_ATTRIBUTE_MODIFIED_EVENT

  • HCI_LE_CONNECTION_UPDATE_COMPLETE_EVENT

  • HCI_ENCRYPTION_CHANGE_EVENT

  • ACI_GAP_PAIRING_COMPLETE_EVENT

But I did not receive these events.

My question is that is the firmware of my bluetooth module STM32WB05N working properly? what else do I need to do to make the pairing work? 

Here's a snippet of my serial log to give you an idea on my issue:

[2025-11-20 15:57:32.929] [COMM][BT] Advertising enabled
[2025-11-20 15:57:32.933] [HCI][INFO] Sending AciGapSetAdvertisingEnable Command
[2025-11-20 15:57:32.933] [DCT][HCI][TX] 01 AC FC 06 01 01 00 00 00 00
[2025-11-20 15:57:32.941] [DCT][HCI][RX] USART RX 1 (7 bytes)
[2025-11-20 15:57:32.941] [DCT][HCI][RX] 04 0E 04 01 AC FC 00
[2025-11-20 15:57:32.941] [HCI][INFO] Event: Command Complete
[2025-11-20 15:57:32.945] [COMM][BT] GATT services initialized
[2025-11-20 15:57:32.945] [COMM][BT] *********************BLUETOOTH READY FOR PAIRING******************
[2025-11-20 15:57:32.945] [COMM][BT] ✓ Bluetooth advertising enabled - ready for pairing
[2025-11-20 15:57:32.945] [COMM][BT] Device should now be visible to mobile phones
[2025-11-20 15:57:32.949] [COMM][BT] ******************************************************************

[T+00:01:33.660] [BLE][ISR] RX IDLE detected, len=50: 04 3E 1F 0A 00 01 08 01 00 6B AF E8 94 9E F8 00 00 00 00 00 00 00 00 00 00 00 00 30 00 00 00 C0 03 01 04 3E 06 12 00 00 01 08 00 04 3E 04 14 01 08 01
[2025-11-20 15:58:43.406] [COMM][BT][DEBUG] Processing 50 bytes: 04 3E 1F 0A 00 01 08 01 00 6B AF E8 94 9E F8 00 00 00 00 00 00 00 00 00 00 00 00 30 00 00 00 C0 03 01 04 3E 06 12 00 00 01 08 00 04 3E 04 14 01 08 01
[2025-11-20 15:58:43.406] [COMM][BT][DEBUG] LE Meta Subevent: 0x0A
[2025-11-20 15:58:43.406] [COMM][BT][DEBUG] Enhanced Connection Complete - Status: 0x00, Handle: 0x0801
[2025-11-20 15:58:43.406] [COMM][BT][DEBUG]   Role: Peripheral, Peer: F8:9E:94:E8:AF:6B
[2025-11-20 15:58:43.410] [COMM][BT][DEBUG]   Interval: 48 (60.00 ms), Latency: 0, Timeout: 9600 ms
[2025-11-20 15:58:43.410] [COMM][BT] ✓ BLE Connection established (0x0801)
[2025-11-20 15:58:43.410] [COMM][BT] Initiating pairing...
[2025-11-20 15:58:43.410] [HCI][INFO] Sending AciGapSetSecurity Command
[2025-11-20 15:58:43.414] [DCT][HCI][TX] 01 8D FC 04 01 08 02 01
[2025-11-20 15:58:43.417] [DCT][HCI][RX] USART RX 1 (7 bytes)
[2025-11-20 15:58:43.417] [DCT][HCI][RX] 04 0E 04 01 8D FC 00
[2025-11-20 15:58:43.421] [HCI][INFO] Event: Command Complete
[2025-11-20 15:58:43.421] [COMM][BT] Pairing request sent
[2025-11-20 15:58:43.769] [COMM][BT][DEBUG] Processing 7 bytes: 04 05 04 00 01 08 3E
[2025-11-20 15:58:43.769] [COMM][BT][DEBUG] Disconnection Complete - Handle: 0x0801, Reason: 0x3E [SUCCESS]
[2025-11-20 15:58:43.769] [COMM][BT] BLE Connection closed (reason: 0x3E)

 

After I received the event HCI_LE_ENHANCED_CONNECTION_COMPLETE_EVENT, I tried to send ACI gap set security command to force to initiate the pairing but still not getting the expected events.

Thanks in advance.

0 REPLIES 0
Announcement

We’re moving the ST Community to a new platform to give you a better and more reliable community experience.