STEF01 Current Limiting Resistor Value
What is the recommended RLIM value for Vout of 28V and Iout of 60mA?
Discuss power management solutions. Ask questions and find answers on voltage configurations, short circuit protection, and programming.
What is the recommended RLIM value for Vout of 28V and Iout of 60mA?
Im planning to use the LDO LD39015M12R with 1.8V Vin, VOut=1.2V 5mA load current. the drop out voltage is 80mV but the datasheet shows the condition of Vin= Vout+1v in the electrical characteristics table.My case will not meet this Vin=Vout+1V condi...
Dear Community,using the STEVAL-ILL089V1 board we would like to power a string of 12 LEDs (Cree XLamp Element G LED Data sheet) and use the PWM dimming function. While the respective raising and falling DIM treshold voltages are clearly stated in the...
Hello,I would like top know if twop LDL212DR regulators can be used in parallel as below. Do you recommend a power pad if I have a 12V ionput and a 6V 150mA output?best regards
Posted on March 23, 2017 at 12:31I tried to connect the EVAL-STPM32 board to the STPM3x Evaluation Software but encountered the following error when trying to read data.Error message: 'Read buffer length insufficient. The operation has timed out.'PC...
The description of the on and off pins is not complete. What happens if both are active at the same time? Does one pin have higher priority than the other? Is it possible to turn the device on/off just using one of the pins letting the other one unco...
Hola, ¿Me podéis ayudar con mi problema? Cuando conecto la realimentación del optoacoplador a RFmax el transformador hace ruido, se regula correctamente la tensión pero el transformador hace ruido. He variado los valores de Rfmin y Rfmax, también los...
Is it possible to start either of these Vipers up earlier than their stated HV startup voltage by sourcing VCC manually (external supply) from the Vin voltage?
Hello, I am currently reviewing your design guide.Could you share the BOM and PCB Layout for this guide?I am interested in the information regarding the part labeled as U1 in the document.
Hi,Trying to develop a board that provide power to a tablet, charger, and the tablet manage the device connected to board.If don't wrong STUSB4500 manage the power flow using CCx lines and over D+, D-, Vbus and GND the device "talk" with tablet and h...
We’re moving the ST Community to a new platform to give you a better and more reliable community experience.