Power management

Discuss power management solutions. Ask questions and find answers on voltage configurations, short circuit protection, and programming.

cancel
Showing results for 
Search instead for 
Did you mean: 

Forum Posts

Resolved! Marking for LD56020M180R

Hi,The part# LD56020M180R Marking is 5618, is it correct? because i unable find the marking info from datasheet for this part, please see the photos of product below, thanks.  

LD56020M180R.png
CW2 by Associate
  • 1151 Views
  • 1 replies
  • 1 kudos

Resolved! STEVAL-WBC86TX Coil change

Hello everyone, I am working on a wireless charger based on the STEVAL-WBC86TX, but we cannot find availability for the transmitter coil reference 760308111 among its components. We would like to know which other references would be compatible with t...

DEIQO by Associate II
  • 1386 Views
  • 2 replies
  • 1 kudos

ADP5091 using TEG

Hello, I would like to use the converter SPV1050 in a new product of my company but I have some doubts. First of all, the application I need is to feed a harvesting device, which includes a supercapacitor of 5F and 5V. So, I need an output from the S...

AGP by Associate II
  • 717 Views
  • 0 replies
  • 0 kudos

Query on Using STM6601 for EN deassertion

Please confirm, for enable deassertion by long press, PB need to be pressed or both PB and SR needs to be pressed. The datasheets mention two things, Note: I need to achieve EN deassertion by long press with one button and INT pin is not connected to...

sanjay1_0-1737363876385.png sanjay1_1-1737363928129.png
sanjay1 by Associate
  • 715 Views
  • 0 replies
  • 0 kudos

Query on Using STM6601 for Single Button Power Control

I am planning to use the STM6601 in my design, which involves powering on with a single press and powering off with a long press. However, my device only has one button. I want to implement a long press to turn off the device, but based on the diagra...

sanjay1_1-1737362756599.png
sanjay1 by Associate
  • 725 Views
  • 0 replies
  • 0 kudos

Unknown Command "DC 0C" while programming STPMIC1A

While programming the STPMIC1A with the USBSTICK – I2C to USB interface, I logged the I2C communication with an oscilloscope. This showed a command "Write, 66, DC 0C" that was send to the STPMIC just before the command to write the shadow registers t...

Resolved! led2001 Resistive load

I am willing to drive a 0.1OHM resistive lead with 4A.Can It be done? eDesignSuite notes that it is possible.I am getting only ~1.4 Amps in my setup

niko-bq by Associate
  • 2000 Views
  • 1 replies
  • 0 kudos

SPV1050 Mode Issue

I am designing a PV cell charging circuit with SPV1050.When the configuration is set to boost mode, I am curious what happens if a voltage higher than Veoc is applied to the PV cell.

Announcement

We’re moving the ST Community to a new platform to give you a better and more reliable community experience.