cancel
Showing results for 
Search instead for 
Did you mean: 

ADP5091 using TEG

AGP
Associate II

Hello,

 

I would like to use the converter SPV1050 in a new product of my company but I have some doubts. First of all, the application I need is to feed a harvesting device, which includes a supercapacitor of 5F and 5V. So, I need an output from the SPV1050 to feed my electronic device, let's say I just need a positive pin and negative pin with an output of 5V. Where I should connect the positive pin of my electronic? In BAT or STORE pin?

Another question is how I can configure the output to 5V.

If you could tell me the configuration I need to perform if I use the STEVAL-ISV019V1I would be very gratefull.

 

Thank you.

0 REPLIES 0
Announcement

We’re moving the ST Community to a new platform to give you a better and more reliable community experience.