Power management

Discuss power management solutions. Ask questions and find answers on voltage configurations, short circuit protection, and programming.

cancel
Showing results for 
Search instead for 
Did you mean: 

Forum Posts

Is it possible to use L9963E daisy chain without L9963T?

 I'm using a single L9963E and it works fine. However, I couldn't start daisy chain connection. When I consider BMS architectures in datasheet, all of them has L9963T transceiver to communicate with further IC. My custom PCB doesn't provide L9963T.So...

berg0vic by Associate
  • 1383 Views
  • 2 replies
  • 1 kudos

L6227Q / L6226Q use with PWM at control inputs

Hi everyone,we're currently using the L6227Q as a driver for 2 DC motors. Everything seemed to work fine. We put on 3,3V on the VREF_x inputs. Enable the IC with EN_x to high and apply a PWM (100 kHz) at the IN1_x and IN2_x. With the PWM (depending o...

Resolved! TS339I

Hi, Team   We are facing issues with test process performed at ICT test station. We are testing driving current to detect Zener Clamp diode 8.2V, the units fail with 2.64688 volts, but this line is connected to comparator TS339I pin 5 that is not pow...

omarvario by Associate II
  • 2254 Views
  • 4 replies
  • 1 kudos

Resolved! VN5T016AH-E

Hi all.I would like to use the VN5T016AH-E high-side driver and I have some questions.*Are there 8V in the CS pin under fault conditions?*Can it measure max 4.2A with a K about 4240? Why do you specify 4V in the datasheet without knowing the value of...

bestyeng_0-1737207651002.png
bestyeng by Associate II
  • 4496 Views
  • 2 replies
  • 1 kudos

L9369 dual channels for one motor

The L9369 is dual channel solution for two rear wheels brakes actuators, but we need only 1 channel for one motor.  Is there special design to combine two channels to drive one motor? If there is single channel EPB driver chip similar to L9369, L9369...

haihun by Associate II
  • 829 Views
  • 1 replies
  • 0 kudos

Resolved! L9963E Current measurment

Hi I have some queries regarding the current measurement function for L9963E. @AScha.3 1) Can we change the gain of current sense or is it a fixed gain and what is the gain error ?2) What is the % overcurrent measurement error ? Can we set the overcu...

David_P_0-1737566160163.png
David_P by Associate
  • 910 Views
  • 1 replies
  • 0 kudos
Announcement

We’re moving the ST Community to a new platform to give you a better and more reliable community experience.