2025-01-13 6:29 PM
I am designing a PV cell charging circuit with SPV1050.
When the configuration is set to boost mode, I am curious what happens if a voltage higher than Veoc is applied to the PV cell.
2025-01-17 5:27 AM
Well, the data sheet states in table 4, parameter VIN_LV for boost configuration a range of min VEN_TH and max VEOC. In addition, table 2 (absolute max ratings) mentions a value of VSTORE+0.3V for IN_LV. You must therefore ensure that this range is not exceeded.
Hope that helps?
Regards
/Peter
We’re moving the ST Community to a new platform to give you a better and more reliable community experience.