Power management

Discuss power management solutions. Ask questions and find answers on voltage configurations, short circuit protection, and programming.

cancel
Showing results for 
Search instead for 
Did you mean: 

Forum Posts

Motor acts as generator and damages VNHD7008AY

We use the VNHD7008AY to control the motor of a cargo lift. The lift has an emergency switch, which disconnects the battery from the circuit.In case of an emergency cutout, the lift runs down while its motor generates a high voltage, which finally ki...

Marc1 by Associate III
  • 1355 Views
  • 2 replies
  • 0 kudos

Resolved! LDL212PUR LDO ceramic caps and resistor values

Hi,I want to buy LDL212PUR LDO. I have 2 questions:1. Can it work reliably with ceramic capacitors?2. What are the recommended resistor values for voltage adjust version?I cannot find this information in the datasheet.Thanks,Adam

awocrf by Associate III
  • 1002 Views
  • 1 replies
  • 1 kudos

Resolved! About the TS3330AMR

The TS3330AMR has a voltage reference, but the internal configuration of the IC is unclear.Is a reverse bypass diode, like the reverse voltage protection of a linear regulator, unnecessary?

Ikegawa by Associate
  • 991 Views
  • 1 replies
  • 1 kudos

stspin32g4 buck converter for Vbat 15V (4s)

hello comunity,i want design a motor controller with the stspin32g4.i have a question about the build in buck converter:i want use the stspin32g4 just with a 4s battery ca 15V and a 2 wire control ifc (servo pwm + ground).I want the stspin32g4 genera...

frankers by Associate II
  • 811 Views
  • 0 replies
  • 0 kudos

3phase metrology FW for STPMS2

Hello, I whant to build a 3 phase meter from the EVALSTPM-3PHISO. The Data that is computed should be send to a display interfacing with an lcd1602 (HD44780). Later a graphical display will be used. But to get a product that is working we have to han...

Tine1994 by Associate II
  • 718 Views
  • 0 replies
  • 0 kudos

VN5T016AH-E low inductance/resistance shorts

Does the VN5T016AH-E handle short circuits with extremely low inductance/resistance without damage to the device? The datasheet states that there is a 53us turn-off delay which would result in 4J of energy in the FET in the case of a dead short with ...

liampwll by Associate III
  • 586 Views
  • 0 replies
  • 0 kudos

DC Motor Driver to generate constant Torque

Hello all, I am writing to inquire about a DC motor driver solution suitable for our application. We are currently using a DCX32L motor rated at 12V and 160W, and our main objective is to achieve constant torque, even during stall conditions. To this...

spolaka by Associate
  • 523 Views
  • 0 replies
  • 0 kudos
Announcement

We’re moving the ST Community to a new platform to give you a better and more reliable community experience.