2025-02-25 9:37 PM
Does the VN5T016AH-E handle short circuits with extremely low inductance/resistance without damage to the device? The datasheet states that there is a 53us turn-off delay which would result in 4J of energy in the FET in the case of a dead short with no input or output inductance ((36V)^2/16mohm*53us), which seems like it would completely destroy the device. We have enough polymer caps on our boards that we could realistically put a few joules in to the FET, so we'd like to know if we need to add some inductance.
We’re moving the ST Community to a new platform to give you a better and more reliable community experience.