Power management

Discuss power management solutions. Ask questions and find answers on voltage configurations, short circuit protection, and programming.

cancel
Showing results for 
Search instead for 
Did you mean: 

Forum Posts

BLDC Motor Control

I am using STGIB30M60TS-L for my BLDC motor control. But when  i am turning the motor ON , the current is increasing continuously resulting in overcurrent error. I am unable to find out where the error is present .How to find it out . I am using TSV9...

hu88 by Associate II
  • 1499 Views
  • 2 replies
  • 0 kudos

Resolved! STEL12H24 RBleed Calculation

On the STEL12H24, but am not sure about the calculation for Rbleed:I am designing a 12V system.RBLEED [kΩ] = VIN / 20 – Rb (min)Rb would be about 95Ω (from Figure 14 in the datasheet)That would make Rbleed 12/(20-95) = -160Ω (negative makes no sense)...

Resolved! Component identification

Hello. I need help to identify this ST component. I can see the ST logo top left. Text is like this from what I see:"ST      (some marking)   G CHG3      648"  

DenDanne_0-1741251508588.png
DenDanne by Associate II
  • 2285 Views
  • 1 replies
  • 0 kudos

L9369-tr IC is not responding.

One of our project we are using L9369-tr IC and we are trying to communicate with the IC using TC38X controller with SPI protocol. We are able to send the data but IC is always giving 0x8efffff6 data as a response and it is not valid data.   Could yo...

Resolved! BULK ID

Can I find the manufacture year from the bulk ID? Most of ST parts only indicate the last digit of the year, sometimes we just don't know it is 2013 or 2023. 

L7987L Failure

Hi, we are using L7987L IC top generate -15V from 24V input. However, we see repetitive failure in the IC. I have attached the waveform also (Green- Input Voltage, Pink- Vout). I am also sharing the layout for the same. Switching frequency we have ke...

Shivalee_0-1740635923190.png Shivalee_1-1740635934131.jpeg Shivalee_2-1740636171581.png
Shivalee by Associate II
  • 3008 Views
  • 6 replies
  • 0 kudos

STEVAL-DPSTPFC1 source code and BINARY code

hello,I have STEVAL-DPS334C1 and STEVAL-DPSTPFC1. I am trying to put PFC code on STEVAL-DPS334C1 again. I load bin file via stm32programmer. then STEVAL-DPS334C1 crashes. I need source code to find where the error is coming from. Or if you have any s...

STEVAL-DPSTPFC1 Hardware Problem

Hello.When I measure between 5V_SCR1 and GND_SCR2 in STEVAL-DPSTPFC1 Hardware, I see 9V. And when I start via Switch, it goes into standby mode when the output is unloaded and reaches 300V. It never becomes 400V. I quickly turn the switch to the off ...

Announcement

We’re moving the ST Community to a new platform to give you a better and more reliable community experience.