vn750ps-e input absolute maximum
Posted on January 31, 2017 at 14:03Hi,Can anyone tell me what the maximum voltage is on the input pin (not Vcc) of this part?Thank you in advance.Regards,Frank
Discuss power management solutions. Ask questions and find answers on voltage configurations, short circuit protection, and programming.
Posted on January 31, 2017 at 14:03Hi,Can anyone tell me what the maximum voltage is on the input pin (not Vcc) of this part?Thank you in advance.Regards,Frank
Posted on January 28, 2017 at 23:20I am designing a board with L6206 drivers for solenoids. My board is using connectors with a 3-amp per pin maximum, so I chose the 6206 for its ability to set a conservative 3 amp shutdown limit on the high side u...
Posted on January 28, 2017 at 09:48Hi. I am Ph.D. Student work on design, analysts and contrl 5-Phase PMSM mtor. I used STGIPS20C60 SLLIMMâ„¢ small low-loss intelligent module IPM, 3-phase inverter - 20 A, 600 V short-circuit rugged IGBT to feed thi...
Posted on January 11, 2017 at 09:17Hello,how can i reset a fault in Firmware?i tried MCI_FaultAcknowledged(oMCI), but it doesnt work.with friendly greetingsEric
Posted on September 28, 2016 at 23:34 hi i am working on lighting dimmer.i want to protect triac when load is short. so how can i do ????? thank you #triac
Posted on January 11, 2017 at 09:13Hello,where can i change the MCU Clock to 16MHz?In the Workbench its not possilbe.Can i change the Value in the Control Stage Parameters.h file?/* ext. clock frequency */#define EXT_CLK_8_MHZto#define EXT_CLK_16_MH...
Posted on January 23, 2017 at 17:44What's going on with the PowerSTEP01s? Seriously, it's been over a year since they went into production yet every distro who sells them are reporting manufacturing delays, and when you contact them it's the same ol...
Posted on December 27, 2016 at 21:18Project: Make one full bridge (non-isolated) rectifier, using two L6491EVAL boards as the gate drivers (the switching transistors mounted to them are FCH190N65F). Initial testing approach: test the full bridge re...
Posted on January 20, 2017 at 10:59Hello,I have to design a 180V/ 2A brushed dc motor controller board using Hbrdige.My question : is there any high voltage ST eval board for brushed dc motors ?If not, is there a low cost solution to obtain 180V DC ...
Posted on November 30, 2016 at 08:24The releaseSW command is behaving erratically.We have our own PCB based on ST design. On Power up GoUntil is executed. Limit Switch used is Omron EE-SX951-W. GoUntil never fails and SW input is detected correctly ...
We’re moving the ST Community to a new platform to give you a better and more reliable community experience.