Power management

Discuss power management solutions. Ask questions and find answers on voltage configurations, short circuit protection, and programming.

cancel
Showing results for 
Search instead for 
Did you mean: 

Forum Posts

VND7140AJ-E Max current

Posted on June 08, 2016 at 11:29Hello All,i have a question about the VND7140AJ-E which i have incorperated into a design of our company. I read the datasheet several times, because the maximum current of the chip is not really stated as such, just ...

michel2 by Associate
  • 1040 Views
  • 1 replies
  • 0 kudos

VNH7013XP-E H-Bridge Datasheet Questions

Posted on January 13, 2017 at 02:26I am having difficulty discerning information from the datasheet.1) Where can I find additional information on this IC? (Other than the OrCad Model and Application Sheet.)2) What voltage can be used to activate/tri...

Tom Dunn by Associate II
  • 1186 Views
  • 2 replies
  • 0 kudos

How to prevent the L298 from heating?

Posted on February 03, 2017 at 11:30Hello, I am using L298N motor driver in parallel mode.But while running the motor L298N IC heats too much and suddenly stop. Motor specification are as follows:- Voltage=12V, Stall current=50A, Rated current=5A. C...

Timing capacitor of L6699

Posted on February 03, 2017 at 11:05Hi, everyoneI encounter a problem about L6699.The sch of L6699 is shown as below.I'm testing in open circuit, so thePC817 is open and all other parameters as shown in the figure.1.The delay is disabled.2.STBY(I'm ...

0690X00000606EIQAY.png

STPM01 STPM10 STPM34 Zero Crossing Signal (ZCR) latency

Posted on January 22, 2017 at 16:34What is the ZCR signal latency with respect to the line voltage for the STPM01 or STPM10?Is the ZCR delay really 5ms for the STPM32 family with respect to the line voltage?thanks,Bruck#stpm34 #stpm10 #stpm33

Resolved! L6472 Stepper Driver Layout Question

Posted on January 26, 2017 at 16:29I notice that the EVAL6472 is a 4 layer PCB.  Similarly, sparkfun has an evaluation board for the L6470 that is also a 4 layer PCB.  My question:  Is there some significance or layout best practice that requires a ...

Saleem by Associate II
  • 1290 Views
  • 2 replies
  • 0 kudos

L6235 commutation scheme

Posted on January 31, 2017 at 10:34We got a problem with a specific motor:With the standard connection one direction of rotation has a significant lower torque and also at 2 specific hall sensor states the current to the coil is switched off !Changi...

gspoerl9 by Associate
  • 1358 Views
  • 2 replies
  • 0 kudos
Announcement

We’re moving the ST Community to a new platform to give you a better and more reliable community experience.