Power management

Discuss power management solutions. Ask questions and find answers on voltage configurations, short circuit protection, and programming.

cancel
Showing results for 
Search instead for 
Did you mean: 

Forum Posts

led600 compensation problem

Posted on January 20, 2017 at 08:42Hello everybody,We have a problem about led6000's compensation, Can anybody advise me about this subject (documentaion, consideration ...etc.) ?  

LD3985 question

Posted on January 19, 2017 at 21:03Hello to all!I have one more question about LD3985. I didn't find any information about limitations in high current modes. Output current of LD3985 is 150 mA. Can I use it for 250 mA load (for example) in continuou...

Preventing/Limiting inrush current on L7986

Posted on January 12, 2017 at 08:51Hi AllI am currently testing a power supply system with a bulk power supply backplane (30V, 12A) and cards that slot in on the backplane. The cards come in various different flavors (24V, 12V, 5V) all using L7986A ...

PWM Timer after Motor Stop

Posted on January 05, 2017 at 13:09Hello,have a little Problem with the Timer (TIM1) on my IHM001I want to brake the motor down to zero and then i want to align the motor to different positions like a stepper motor.The Braking down to zero works, th...

s61331 by Associate II
  • 940 Views
  • 1 replies
  • 0 kudos

Resolved! LED1642GW series connection, brightness.

Posted on January 09, 2017 at 00:16I try use two drivers. I can switch on/off any output channel, but I can't use brightness registers correctly. Manual has description how work with one driver. But if I send brightness data to first driver, a secon...

Question about HALL_CalcAvrgElSpeedDpp function

Posted on January 09, 2017 at 04:53I notice  wAux = pDVars_str->wPseudoFreqConv /pDVars_str->SensorPeriod[pDVars_str->bSpeedFIFOGetIdx].wPeriod; hAvrgElSpeed = (int16_t)(wAux); hAvrgElSpeed *= pDVars_str->SensorPeriod[pDVars_str->bSpeedFIFOGetIdx].b...

Troubleshooting with spv1040 MPPT

Posted on December 09, 2016 at 03:38Hi,We designed a battery charger using SPV1040. The output voltage is fine;however, during the charging process, there is a large fluctuation on the input voltage : 500mV ~ 1V. Ideally. This input voltage should ...

0690X00000605oeQAA.png

Energy Harvesting - SPV1050 setting MPPT

Posted on December 08, 2016 at 11:59I have a range of ideas that I want to try using a motor and movement as a generator. Can I omit the MPPT resistors from my circuit and still use the IC as a battery management and linear regulator?Secondly when I...

Announcement

We’re moving the ST Community to a new platform to give you a better and more reliable community experience.