2016-11-29 11:24 PM
The releaseSW command is behaving erratically.
We have our own PCB based on ST design. On Power up GoUntil is executed. Limit Switch used is Omron EE-SX951-W. GoUntil never fails and SW input is detected correctly all the time.After GoUntil, ReleaseSW and Move are executed. Sometimes (unpredictably) ReleaseSW and Move are not executed. Appreciate inputs for trouble-shooting this behavior.2017-01-20 1:53 AM
When the algorithm fail, are both ReleaseSW and Move not executed?
I suggest you to check the following:
- The SW_MODE you set. By default a falling edge on the SW input causes an abrupt stop of the motor (hard-stop).
- The status of the SW input before you send the ReleaseSW command. The ReleaseSW stops the motor only at the SW input
RISING EDGE
. If the SW input is high, the command continues driving the motor (at very very low speed) until it falls low ad then returns high.- The status of the BUSY pin/flag before sending the Move command. It is not possible to send a move when the device is busy.
We’re moving the ST Community to a new platform to give you a better and more reliable community experience.