Power management

Discuss power management solutions. Ask questions and find answers on voltage configurations, short circuit protection, and programming.

cancel
Showing results for 
Search instead for 
Did you mean: 

Forum Posts

STUSB4500, how we can set profile through I2C using nrf52832 MCU.

Hello, I am using STUSB4500 Type C IC , I want to set the profile for 5V 3A.I referred the code given in Github:https://github.com/usb-c/STUSB4500Same we have implemented in nrf52832 SDK, but its not getting programmed.Any solution for this? How we ...

HJada by Associate
  • 1148 Views
  • 1 replies
  • 0 kudos

VNH7100AS pull down resistor

Hello, do the INA INB and PWM pins have an internal pull down resistor?In the examples you connect these pins with a 1k resistor directly to the microcontroller, but if you do not have a pull down resistor you may be fluctuating at the start of the m...

What do I need to evaluate the powerstep01 ?

We are starting to use your L6470 drivers and used the EVAL 6470H pcb for evauation . I found it very usefull during the development especally being able to see the values in all the registers .It would be helpful if I could do the same with the powe...

GFOST by Associate
  • 803 Views
  • 0 replies
  • 0 kudos

We want to control and drive a 2 poles 1.5A 12v BLDC motor at PWM switching freq. of 50Khz and 19.000 rpm with a 15cm2 PCB space available. Would you like to recomend the most suitable device set?

We Checked the STSPIN32F0 and the PWM was limited to 30KhHz with overclock, we don´t found any easy way to increase PWM freq.The objective is to obtain the maximum performance of the motor with the minimum heat disipation

JPALOUF by Associate
  • 730 Views
  • 0 replies
  • 0 kudos

STBB1-APUR minumum voltage

Hi,I have a STBB1-APUR in a circuit with a battery. As I can see, it will lower down the voltage from by battery to 3.3V, but it will also boost it to 3.3V if the battery has lower voltage. Is there any way to disable the boost? I would like to close...

Overcurrent fault always set without PWM enabled.

I have a 446re nucleo and IHM07M1. I am just trying to get my 6 step BLDC with Hall sensors to work. My overcurrent PIN 'PA6' is set all the time. As soon as i turn on 12 V DC to IHM and USB to nucleo , i read the PIN as HIGH. I have measured the vol...

MKuls by Associate
  • 662 Views
  • 0 replies
  • 0 kudos

This is a question about the signal name of VIPer22A.

I am repairing the power supply of AC-DC5V. According to the VIPer22A data sheet, pins 5-8 are "DRAIN" It was confirmed that the purchased VIPer22A has the same pin number 5-8. However, the VIPer22A (4PY138) used for the AC-DC5V power circuit purchas...

michi.278 by Associate II
  • 1931 Views
  • 1 replies
  • 0 kudos
Announcement

We’re moving the ST Community to a new platform to give you a better and more reliable community experience.