Discuss power management solutions. Ask questions and find answers on voltage configurations, short circuit protection, and programming.
I have seen other products similar to this one from other suppliers that can work in this configuration in addition to the flyback topology. Can this part be used in a buck topology?
Dear communityI have developed a bldc motor driver using a DRV10983 chip from texas instruments target speed 3000.00 RPMIt works of BEMF and dose not use hall effect sensorsI have achieved good stability but the instrument the motor is designed for n...
Dear Sir or Madam,we use the DC-DC Converter L5973D in some circuits and i want use it in the future, too. To do it easier I prove the circuit with a LT-Spice based programm.Now my problem is, that your offer a encrypted Pspice-Model. It is possible ...
Hello,I am trying to control L6470 mounted on IHM02A1. I downloaded the example software (https://www.st.com/content/st_com/en/products/embedded-software/mcu-mpu-embedded-software/stm32-embedded-software/stm32cube-expansion-packages/x-cube-spn2.html#...
The eDesignSuite result and my schematic are attached. A PCB was manufactured as per the eDesignSuite BOM and design guidelines. I connected mains to the circuit without SJ4 being bridged. Rin immediately blew. The design BOM specified a 7.5Ω , 2W re...
Hi,[1] Is this board supported for automatic code generation in MATLAB/SIMULINK ? [2] How high must the electrical rotary field resolution be for FOC operation, if I want to operate the PMSM without an observer? [3] Is it possible to switch the opera...
When trying to set up a simulation in E-Design, the highest input voltage that can be input is 265?If this can be used at 480 VAC as I suspect, how do I get the voltage settings on the E-desgn tool revised
I have looked at the evaluation module and the datasheet i can't spot where restriction for sinking voltage are discussed. Please advice on this because i need to utilize this STUSB1600 ICThanks
We’re moving the ST Community to a new platform to give you a better and more reliable community experience.