2019-12-03 2:09 AM
Hi,
I have a STBB1-APUR in a circuit with a battery. As I can see, it will lower down the voltage from by battery to 3.3V, but it will also boost it to 3.3V if the battery has lower voltage. Is there any way to disable the boost? I would like to close all the circuit if the battery is less than 3.5V because the boost is killing by battery.
We’re moving the ST Community to a new platform to give you a better and more reliable community experience.