2019-11-17 3:06 PM
I have looked at the evaluation module and the datasheet i can't spot where restriction for sinking voltage are discussed. Please advice on this because i need to utilize this STUSB1600 IC
Thanks
2019-12-05 5:53 PM
Hello,
The STUSB1600 is a USB Type-C controller only. It doesn't support USB Power Delivery (PD) mode.
A USB-Type-C controller can only get or provide 5V/3A maximum.
If you want to get a higher voltage (up to 20V), then you'll need to use a controller which support USB-C PD.
For instance, you can use one of the following solutions, which support USB PD and DRP:
- STM32G0x + TCPP02
- STM32G4x + TCPP02
- STM32F0x + STUSB1602
Best regards.
We’re moving the ST Community to a new platform to give you a better and more reliable community experience.