Discuss power management solutions. Ask questions and find answers on voltage configurations, short circuit protection, and programming.
I am designing a Isolated Flyback SMPS with input range upto 1KV and output of 20W. I couldn't found any flyback controller which will support this range. I found one offline PWM controller named STCH03 which is having limited 650V start-up.So is it ...
We expect to got the same ID cause the devices is the same and the only difference is the battery voltages.
For documentation purposes i need to estimate the worst case temperature for the powerSTEP01 that occurs in our application. I already calculated the worst case power dissipation so i am able to determine the temperature with information about the "j...
Hello CommunityRecently I'm in a project with the NUCLEO-G071RB.I been working with ST boards for a long time but this time, i cant make measurements through specific channel "ADC_IN15". Pin PB11I made other channels to work ( IN0, IN1 etc...) but w...
Hello,The 600mA current available on STSPIN32F0's gate drivers seems too low for high current applications.Does ST or anyone, could suggest any 'buffer' to increase that current?Thank you!
Hello,I have a custom board with a STC3117 as the fuel gauge to a 5200mAh lithium ion battery pack. The pack can charge up to 1.5A and discharge to up to 3 A. The issue I am seeing is that the SOC will be stable with the system running. When I charge...
We're planning to develop some motor drive academic boards for SMPMSM FOC motors for Master Students and for one of the parts we're using is STEVAL-IHM023V3. We're currently development the platform.In the manual UM1823, page 28, table 6 for FOC cont...
We’re moving the ST Community to a new platform to give you a better and more reliable community experience.