Power management

Discuss power management solutions. Ask questions and find answers on voltage configurations, short circuit protection, and programming.

cancel
Showing results for 
Search instead for 
Did you mean: 

Forum Posts

Basic Model vs. Electro-thermal Model of TVS Diodes

Hello,I have some questions about ISO7637-2 and ISO16750-2 transient pulse simulations using the basic model and the electro-thermal model of TVS diodes in LTspice.1) In a DC sweep simulation, I observed different IV characteristic curves between the...

WonnyPa_0-1757658731503.png WonnyPa_1-1757658752940.png WonnyPa_2-1757658840833.png WonnyPa_3-1757658856297.png
WonnyPa by Associate
  • 609 Views
  • 0 replies
  • 0 kudos

STEVAL STWBC86TX programming

Hello, I would like to program a board with the initial configuration of the STEVAL STWBC86TX. To do this, I need two files: PATCH and CONFIG. Where can I download these files to the STSW-WPSTUDIO GUI of the test board we have?

DEIQO by Associate II
  • 800 Views
  • 2 replies
  • 0 kudos

Looking for STWBC2-HP Fixed Power Output Firmware

大家好,我目前正在研究基于 STWBC50-HP 芯片的 2W 无线功率发射器。我的目标是在不使用 Qi 协议的情况下验证硬件功能,用于学习和测试目的。我已经完成了发射器硬件设计,现在正在努力寻找一种无需 Qi 通信即可输出固定功率的固件,例如演示或示例项目,例如:STWBC2-FW-固定功率输出、或任何允许恒定功率输出(例如,19V 2.6A)而无需协议协商的类似固件。不幸的是,我在 ST 网站资源或 STM32Cube 软件包中找不到确切的固件。任何人都可以分享下载链接或提供在哪里找到此固件...

ST L4986A not working

We’re currently facing an issue with the L4986A PFC controller in one of our designs. The IC is not functioning as expected, and we would appreciate your guidance.:wrench: Issue Summary:• The IC receives all input voltages within the recommended oper...

Screenshot 2025-09-11 194603.png WhatsApp Image 2025-09-11 at 7.42.39 PM.jpeg

Resolved! STPMIC25 latching

Hello,I'm in the process of moving from MP1 to MP2 on my device. The latter, used STPMIC1 that suffered the startup problem as described in AN5861 and I had to go thru a re-design to include the latching circuit on my PCBA.Can anybody confirm that th...

Internal Gate Resistance of STP150N10F7

Hey everyone, I am trying to derive the internal gate resistance (R_Gint) of STP150N10F7. Can anyone help me with the calculation please. https://www.st.com/resource/en/datasheet/stp150n10f7.pdf   Regards,Vamsi.  

Viper UVP when configured as high-side buck

Hello,We are using Viper31 to step down 250VDC to 12VDC in a buck configuration as shown in Figure 42 of the datasheet:This is also the same topology used in STEVAL-VP319X1B:We are working with STEVAL-VP319X1B to try to implement the UVP function wit...

engineer55_0-1757433775850.png engineer55_1-1757433815520.png
Announcement

We’re moving the ST Community to a new platform to give you a better and more reliable community experience.