Power management

Discuss power management solutions. Ask questions and find answers on voltage configurations, short circuit protection, and programming.

cancel
Showing results for 
Search instead for 
Did you mean: 

Forum Posts

VND5T016ASP-E High Side Driver IC Hardware Design

Hello everyone,I would like to use the VND5T016ASP-E high-side driver in my design.For one board, I need to use 12 of these ICs.I have reviewed the application note; in your opinion, which configuration should I use for this IC to have fewer EMC issu...

Resolved! L6920DB temperature range

The L6920DB temperature rating is not specified in the datasheet. However, it gives the temperature data as Max Tj=150C, Thermal resistance is 180C/W. Based on Tj=Ta+Pd*ThetaJa, if Ta=85C, then the Pd allowed in this temperature is very low. Is L6920...

qwhus by Associate II
  • 1288 Views
  • 5 replies
  • 1 kudos

STEVAL-ISV019V1 High Battery Current

Hello!I am attempting to charge a 3.7 V Li-ion battery using the SPV1050 on the STEVAL-ISV019V1 evaluation board, but there is a current coming from the battery into VBATT which ranges from 400 uA to 1 mA.The current remains even when no load is conn...

Resolved! LM2904 PSPICE 's symbol

Dear  engineer             Now, I  want  to  get  the  LM2904's  symbol  to simulate  in the PSPICE.   AS usually  ,  in this window,the symbol will be automaticlly created . but this time ,it  does not be automaticlly  created。Please help me  solve ...

1754989880536.png
PENG66 by Associate
  • 1103 Views
  • 1 replies
  • 0 kudos

Resolved! STWLC38 will not report Ptx correctly

Hello, I am trying to follow the Getting started with the STEVAL-WLC38RX document for FOD tuning attached. I am using STEVAL-WBC86TX, powered from a bench top PSU,  and STEVAL-WLC38RX, connected to an electronic load. Both are connected to the STMGUI...

Resolved! Powering Stm32f407vet6 from metal detector power supply

I have some Pulse induction metal detector analog designs that I want to "digitalize" using a Stm32f407vet6 board. Unfortunately, these designs use the battery positive as ground. My intention is to power the Stm32 from the +5v rail of the detector p...

Recommendations for a Flyback Design Challenge

We are in need of an Isolated Flyback DC/DC Converter design to work with a 24 to 96V battery system. It is to be a 15-140V input to 12V output voltage and, 4-5A nominal 9A peak output current converter. We want to use the Würth transformer "74919654...

Resolved! LDH40PURY

Hi team, We are working for redesign board which should not have any China parts, so we are looking for Non China origin /  manufactured part. Could you please confirm the below details for LDO partLDH40PURY1) Country of origin (Manufacturing / Assem...

Announcement

We’re moving the ST Community to a new platform to give you a better and more reliable community experience.