Power management

Discuss power management solutions. Ask questions and find answers on voltage configurations, short circuit protection, and programming.

cancel
Showing results for 
Search instead for 
Did you mean: 

Forum Posts

Speed Control problem with L6235 DIP

Posted on October 25, 2016 at 20:05Hi All,I want to make a BLDC motor driver board using L6235N DIP.I wired all the components on the breadboard as per schematic diagram and component list is given in ST Application Note AN1625 page no. 35-37.I am u...

vkyadav by Associate
  • 1544 Views
  • 2 replies
  • 0 kudos

Resolved! FDA803S/FDA903S

I need more information about FDA803S on website there aren't document explaining I2C registers and details about connection of configurable pins (eq ENABLE1 an 2) There is a firmware example for use this device connected to a stm32 microcontroller?

BTA24-800CW can't switch off 60 W resistive lump

i am using MOC3063 as an optocoupler and BTA24-800CW as a triac .with 220 V ac and it worked fine (switch on and off) with the 10W,5W,3W resistive loads but when using 60 W incandescent lump it only turn on but not off   i am using this basic circui...

momensalah_0-1753671467464.png

Resolved! STEF01 VCC/GND in a -48V system

Hi Sir, For a system with -48V and 0V (Ground) power rails, can I use the STEF01 with the following connections?Connect the IC's GND pin to the system -48V rail.Connect the IC's VCC pin to the system 0V rail.  Will the chip work correctly and safely ...

TIENHUA_0-1757580574111.png
TIENHUA by Associate III
  • 1650 Views
  • 5 replies
  • 0 kudos

Resolved! [BLDC] How to get trapezoidal back-emf waveform

Hi All,I'm working on driving sensorless BLDC motor by 120 degrees trapezoidal control.I'm stuck on to get back-emf voltage like below figure:My result is like this.And the circuit used for voltage sens part is as follow.I don't know if it's a circui...

0693W000008ztZFQAY.png 0693W000008ztZPQAY.png 0693W000008ztZjQAI.png
Kenji1 by Senior
  • 7966 Views
  • 9 replies
  • 1 kudos

SCT040W120G3AG Spice model incomplete

The SPICE model file for the product SCT040W120G3AG downloaded from the official website is incomplete, it only has the LIB format file. Can someone provide me with the complete SPICE model file? Thank you!

Shanny_ by Associate
  • 1034 Views
  • 0 replies
  • 0 kudos

wireless power transfer

Hello experts!my GP is to design an offline DC/DC converter ( LLC )  for cordless home applainces similar to the attached file, now I am aware of how to design LLC for conventional Chargers (wired) to some extent, but i get compeletly confused when i...

Announcement

We’re moving the ST Community to a new platform to give you a better and more reliable community experience.