Discuss power management solutions. Ask questions and find answers on voltage configurations, short circuit protection, and programming.
I need simple implementation.Hold time for On and hold time for Off can be configured be resistors / capacitors assembly.Could you please suggest for relevant IC?Thanks!Erez
Please provide and diagram or application note on the same.
In the datasheet , all industry level component's operation temperature is invalid. For example, STPS30M100DJF.Traditionally , industrial component's operation temperature is -40~85℃(at least). Without this information, engineers can not make the ri...
I'd like to use STUSB4500 to allow for 20V 60+W to enter the system, but I'd also like to use the sideband pins (or other pins) to send some serial data to the host side. I'd like to know whether this is possible (seems like the chip doesn't use SBU ...
I have this chip on a board LD2985BM50R. how can I verify the mark on top of the chip is marching the chip? it is really funny that the mark wasn't mentioned in the data sheet. Thank you,David
The Vce without load is 7.3V, and once load connected it is 18V. I want know what should be the ideal voltage drop across CE, with load and without condition.Attaching the schematic screen shot for reference.
We’re moving the ST Community to a new platform to give you a better and more reliable community experience.