Discuss power management solutions. Ask questions and find answers on voltage configurations, short circuit protection, and programming.
I need to make a Resonant Inverter, with AC output.Application is an AC power supplyTopology: LLC or otherInput: 12V to 24V DCNo DC output100 kHz100W0 to 20A continuousconstant voltage0 to 5VInductive load for galvanic isolationpure sinesoft-switched...
I have been using the PWD13F60 dual H Bridge IC which is a great device but the EVALPWD13F60 Eval board is limited to 2A_rms even though the IC is good for 8A DC due to thermal limitations of the eval board which is a shame as I really need to get a...
From documentation I can not figure if it is possible. Do you have any configuration of resistors(R4,R5,R6) in order to modify Vuvp and Veoc?
I would also like to know if there is a way to at least cycle the enable pin with a hardware circuit if the part does latch.
We’re moving the ST Community to a new platform to give you a better and more reliable community experience.