2023-05-13 7:15 AM
2023-05-13 9:47 AM
What kind of stepper motors ? if you are talking about the small 5-12V you buy on Aliexpress.
You can use for example L293DNEE4 to interface motor and you program four IO pins on your STM32 chip.
Here is example for the stepper motor, it does not mean it will work with another you need to figure out the sequence how to energize the coils
void forward_single_stepping_stepper_1(uint16_t speed, uint16_t steps)
{
for (uint16_t i = 0; i <steps; i++)
{
HAL_GPIO_WritePin(GPIOA, GPIO_PIN_9, GPIO_PIN_SET);
HAL_GPIO_WritePin(GPIOA, GPIO_PIN_10, GPIO_PIN_RESET);
HAL_GPIO_WritePin(GPIOA, GPIO_PIN_11, GPIO_PIN_RESET);
HAL_GPIO_WritePin(GPIOA, GPIO_PIN_12, GPIO_PIN_RESET);
HAL_Delay(speed);
HAL_GPIO_WritePin(GPIOA, GPIO_PIN_9, GPIO_PIN_RESET);
HAL_GPIO_WritePin(GPIOA, GPIO_PIN_10, GPIO_PIN_RESET);
HAL_GPIO_WritePin(GPIOA, GPIO_PIN_11, GPIO_PIN_SET);
HAL_GPIO_WritePin(GPIOA, GPIO_PIN_12, GPIO_PIN_RESET);
HAL_Delay(speed);
HAL_GPIO_WritePin(GPIOA, GPIO_PIN_9, GPIO_PIN_RESET);
HAL_GPIO_WritePin(GPIOA, GPIO_PIN_10, GPIO_PIN_SET);
HAL_GPIO_WritePin(GPIOA, GPIO_PIN_11, GPIO_PIN_RESET);
HAL_GPIO_WritePin(GPIOA, GPIO_PIN_12, GPIO_PIN_RESET);
HAL_Delay(speed);
HAL_GPIO_WritePin(GPIOA, GPIO_PIN_9, GPIO_PIN_RESET);
HAL_GPIO_WritePin(GPIOA, GPIO_PIN_10, GPIO_PIN_RESET);
HAL_GPIO_WritePin(GPIOA, GPIO_PIN_11, GPIO_PIN_RESET);
HAL_GPIO_WritePin(GPIOA, GPIO_PIN_12, GPIO_PIN_SET);
HAL_Delay(speed);
}
}
so giving you mine library it does not mean it will work in your case.
2023-05-13 1:57 PM
hi, im talking of a motor like Nema 17, i have to controll a simple robotic arm, i searchin some algorithms or a flowchart of the controll so i can convert it in a code... im new to this stuff
We’re moving the ST Community to a new platform to give you a better and more reliable community experience.