Power management

Discuss power management solutions. Ask questions and find answers on voltage configurations, short circuit protection, and programming.

cancel
Showing results for 
Search instead for 
Did you mean: 

Forum Posts

SiC drive

For the SCT10N120 switching tube, I need a switching frequency of 7Mhz, is there any driver chip I can use?

hhh by Associate
  • 1012 Views
  • 1 replies
  • 0 kudos

SPI L9026 frame counter value

good morning, i ave a question. This indication relating to the "frame counter value" appears in the manual of L9026."As additional safety feature, the protocol is also equipped with 1 PARITY bit (odd parity) and a 1 bit frame counter;the frame count...

Resolved! FOD on STWBC-MC

 Hello STM community.We developed a wireless charger based on the STWBC-MC chip.Our design follows exactly the ST Eval-Kit STEVAL-ISB047V1.No we are facing a problem with a customer, that the Foreign Object Detection (FOD) does not work stable. In so...

SvenRaecker_1-1710136601114.png

Resolved! How to evaluate LED7708 with more than 16 channels

I am running a STEVAL-ILL035V1 board using software downloaded from your site.Downloaded software is LED_DRIVER_GUI7708_1.0.1_130722.exe.Then I connected an additional board STEVAL-ILL035V2 and changed SW7 on ...V1.But now I am not able to control th...

0690X000009XfVgQAK.png

Question for Application note AN5734.

My company designs circuits and artwork upon request from customers.We are considering this project based on a customer's request to change the laser power supply to be compatible with worldwide use.While considering various things, I am also conside...

shinba by Associate
  • 1664 Views
  • 2 replies
  • 0 kudos

Resolved! STPMIC1 issue

Hello.We are using the STPMIC1APQR with the electrical scheme shown in the figure.  We are using the outputs corresponding to BUCK4, LDO4, LDO2, and LDO1.The BUCK4 and LDO4 outputs have voltage at startup, however, the LDO1 and LDO2 outputs, although...

PMIC_rtaImage.png
PAkRad by Associate III
  • 2040 Views
  • 2 replies
  • 1 kudos

WLC38RX

We are using WLC38RX and wish to configure register setting usign the STSW-WPSTUDIO . However we do not have the EVK. Can we set the registers in the app and save the file? We need the basic config of 5V supply for battery charging, 100mA normal and ...

plawat by Associate III
  • 1281 Views
  • 1 replies
  • 0 kudos

Resolved! L6472 output voltage detected on motor supply

Hello,      I have a board based on the stepper driver L6472. I noticed that, when I do not provide input 12V for the motor (the motor 12V but I provide the 3.3V for the logic (VREG, VDD, SW), I find a voltage of about 2.6V on the VSA, VSB pins. I tr...

MRaff.1 by Associate III
  • 1423 Views
  • 2 replies
  • 0 kudos
Announcement

We’re moving the ST Community to a new platform to give you a better and more reliable community experience.