Resolved! STEVAL-CTM015V1:3D MODEL NEEDED
Find a 3D model of STEVAL-CTM015V1,THANK YOU
Discuss power management solutions. Ask questions and find answers on voltage configurations, short circuit protection, and programming.
Find a 3D model of STEVAL-CTM015V1,THANK YOU
I am working on steval -L3751V12 boardI am wanting the pcb files/ gerber files of the above demo board. can you help
Hi I am using the X-NUCLEO-LPM01A and is it best to press the calibration button when my own circuit board is not connected, or do I press it after its connected and running? What exactly is it calibrating against?The reset target button, does that...
I am evaluating the VN9D5D20F 4-channel high-side driver for a design (https://www.st.com/en/automotive-analog-and-power/vn9d5d20f.html).According to the datasheet, the PWM clock should be provided via the PWM_CLK input, but there's also this note ab...
Can i use STGAP2SICSA gate driver for silicon MOSFET or can you suggest me AEQ qualified high side smart gate driver with has short circuit current protection with inbuilt charge pump to drive high side MOSFET.
Hi,Is there a solution to use PCB based Rogowski coil with STPM33 from 200 mA to 200 A with 0.2 Class Metering accuracy as per ANSI C12.20
Is there a Spice model of the MC34063? I checked the CAD resources, but I do not see simulation models. Thanks
Hello,I am using the TCPP03-M20, and would like to save space/cost by combining the Source and Sink path into one mosfet gate pair.The datasheet provides an example of a combined source/sink path using two Schottky diodes and a 1M resistor with the s...
Hello,thermal data of the L78M show junction-to-ambient thermal resistance (θJA) and junction-to-case thermal resistance (θJC) for different packages (e.g., TO-220 and DPAK). Those figures differ, of course. Note that the datasheet provides no juncti...
Hi every ones. Where I can found L7915CV negative voltage regulator spice model? Or other equivalent spice model of other negative regulator. I saw that it is obsoleted.
We’re moving the ST Community to a new platform to give you a better and more reliable community experience.