2024-03-11 11:56 PM
My company designs circuits and artwork upon request from customers.
We are considering this project based on a customer's request to change the laser power supply to be compatible with worldwide use.
While considering various things, I am also considering a PFC circuit with L4985.
Question for Application note AN5734.
AN5734 : Table 4 on page 27
Is the relationship between Wire type and Wire diameter correct?
----------------------------------------------------------------------------------------------------------------------
Windings Start pins End pins Number of turns Wire type Wire diameter
PRIM 5 2 70 Single – G2 Litz 0.2Ø x 30
AUX 9 11 5 (spaced) Litz – G2 0.28Ø
----------------------------------------------------------------------------------------------------------------------
Do you have any information on transformers?
Best regards.
2024-03-12 3:19 PM
Welcome @shinba, to the community!
Why exactly do you think the information on wire diameter and wire type is incorrect?
Regards
/Peter
2024-03-13 5:26 AM
The wire type on the PRIM side is single Grade 2, but the wire diameter is Litz wire.
Also, the wire type on the AUX side is grade 2 Litz wire, but the wire diameter is 0.28Φ.
Is this correct.
Best regards.
We’re moving the ST Community to a new platform to give you a better and more reliable community experience.