2025-03-24 10:11 AM - last edited on 2025-03-24 10:14 AM by mƎALLEm
Hi Team,
I am a complete beginner. I am working on a project using STM32F429 DISC1 to drive an external LCD using LTDC (parallel RGB interface) using the ST7789H2 driver. Currently, I have a working code for running the LCD that comes with the discovery board using the ILI9341 driver. How can I port this code to work with an external LCD using ST7789H2 with the same interface?(RGB parallel).
Thanks
Solved! Go to Solution.
2025-03-24 10:15 AM - edited 2025-03-24 10:19 AM
Hello @Shankar_Mohan and welcome to the community,
You can refer to the application note AN4861 "Introduction to LCD-TFT display controller (LTDC) on STM32 MCUs" as it may help you.
You need to read the ST7789 datasheet and implement its driver accordingly.
But are you sure ST7789 is controlled over LTDC not over SPI interface?
See these threads:
https://community.st.com/t5/stm32cubeide-mcus/st7789-not-working/td-p/572930
2025-03-24 10:15 AM - edited 2025-03-24 10:19 AM
Hello @Shankar_Mohan and welcome to the community,
You can refer to the application note AN4861 "Introduction to LCD-TFT display controller (LTDC) on STM32 MCUs" as it may help you.
You need to read the ST7789 datasheet and implement its driver accordingly.
But are you sure ST7789 is controlled over LTDC not over SPI interface?
See these threads:
https://community.st.com/t5/stm32cubeide-mcus/st7789-not-working/td-p/572930
2025-03-24 1:26 PM
Hi,
i am using TFT with ST7789 , but is on SPI connected;
so how is yours connected ?
We’re moving the ST Community to a new platform to give you a better and more reliable community experience.