2015-07-21 2:07 AM
Hello,
I design DC-DC converter using eDisign and I make it with folowing parameters: Vin = 11-14 V Vout = 5 V Iout = 700 mA Design software limits maximal inductance for this IC to 10uH, but then IL ripples are quite big ( around 50%). Can I use it bigger inductance for this IC or it's not possible ? I didnt see any information about it in data sheet.2015-07-28 2:24 AM
Hello,
the e-design is an automatic tool that allows the user to easily realize an application.The tool is utilized to match a lot of different conditions but, to don't increase its complexity, it has been necessary to establish some conditions for the power components.
The condition you have seen on e-design is due to the implementation of the tool, not to a limitation of the device.
The official technical document of the device is the datasheet, following the equations reported it's possible define a working application with a coil value bigger than 10uH.
Following your specs:
-> Vin = 11-14 V
->Vout = 5 V
-> Iout = 700 mA
I have realized on the evaluation board of the device the attached application.
Best regards. ________________ Attachments : Application.png : https://st--c.eu10.content.force.com/sfc/dist/version/download/?oid=00Db0000000YtG6&ids=0680X000006HzDB&d=%2Fa%2F0X0000000bIR%2FlVjVDLeFq8vhTFjOFuwPNVtywBSOBJLT16PkET7szP4&asPdf=falseWe’re moving the ST Community to a new platform to give you a better and more reliable community experience.