2025-04-22 11:25 PM
Hi all,
I'm working with an STM32-based motor control setup ( The EVSPIN32F0251S1 board is a 3-phase complete inverter based on the STSPIN32F0251 controller), and I have a physical PMSM motor that I want to use with FOC (Field Oriented Control).
I need help figuring out the following motor parameters:
Parameters I want to find:
Stator resistance (Rs in Ohms)
Stator inductance (Ls in mH)
Back-EMF constant (in Vrms/kRPM or Vpeak/kRPM)
Maximum mechanical RPM
What I have:
Physical motor only and basic data (no datasheet)
PMSM motor
Volt -24
Current -4.3 amp
Power -105W
RPM - 500 Hz- 83.3 Hz
Pole Pair -10
Torque -2.0 Nm
Can measure with multimeter, oscilloscope, etc.
Using STM32 Nucleo-F446RE board Planning to use STM32 Motor Control Workbench & SDK
My questions: What is the best method to measure Rs and Ls accurately with basic lab equipment?
How can I measure or estimate the BEMF constant?
Is there a reliable way to determine the maximum safe RPM if the motor model is unknown?
Can the STM32 MC Workbench help extract these automatically?
Any guidance, measurement techniques, or scripts/tools would be much appreciated!
Thanks in advance!
Solved! Go to Solution.
2025-04-23 6:36 AM
Hello @Vedant07;
You can use MC Motor profiler tool provided on MCSDK available here. Feature is available using Nucleo-F446RE board.
You can also have a look to How To manually configure the motor parameters link.
2025-04-23 6:36 AM
Hello @Vedant07;
You can use MC Motor profiler tool provided on MCSDK available here. Feature is available using Nucleo-F446RE board.
You can also have a look to How To manually configure the motor parameters link.
We’re moving the ST Community to a new platform to give you a better and more reliable community experience.