2007-03-13 3:26 AM
2007-03-01 1:08 AM
Hi
I have STICK programer and MCu ST7FMC2S6 I want program it by STVP. MCu is unprogramed completly new.In configuration of Visual programer is available only option STICK->ICP mode(not ICP OPT Enable or Disable) for my MCu. How must I conect pins 9 and 7 in header? I tried it by four ways (connected one of them or unconected) but error message was executed> > Blank checking section [8000-DFFF] of PROGRAM MEMORY area... Error : Cannot communicate with the device ! Option Bytes are Enabled on the device. Check the ICC cable connection and check all the needed pin connections on the ICP connector. conectror is good all signals goes throuhh the cable Can someone help me? thanks for reply soonWe’re moving the ST Community to a new platform to give you a better and more reliable community experience.