2014-12-18 2:03 AM
I�m going through this application note on the ST website: http://www.st.com/web/en/catalog/tools/PF258002
The application note states that it comes with source code for an example of an IAP bootloader implementation: �For this purpose, an example of a user-bootloader firmware is provided with this application note. This package is divided into three main subdirectories, each one dedicated to one STM8 family member: STM8AF, STM8L and STM8S. For the STM8AL family, please use the STM8L directory. Each directory is composed of the following components: ? Sources: containing the firmware source code�However, the download link on the same page (STSW-STM8062) only has S19 hex files and no source code. I was wondering if someone could provide me with the source code. Any help would be appreciated. #stm8 #bootloader #iap #stsw-stm32098We’re moving the ST Community to a new platform to give you a better and more reliable community experience.