2023-07-21 5:34 AM
Hi,
Im trying to track down a couple of diodes to repair a card. The markings are EV Z551
It also has the ST logo on it, surface mount.. Anyone know where I can obtain some..
Cheers
Kev
Solved! Go to Solution.
2023-07-21 6:06 AM
Welcome @Jamer, to the community!
Unfortunately, you have not included a legible photo, but if the marking EV is indeed on the device, it is the SM6T36A. By the way: it is not a Zener, but a TVS = Transient Voltage Suppressor.
If the problem is solved, please mark this thread as answered by selecting Accept as Solution, as also explained here. This will help other users find that answer faster.
Good luck!
/Peter
2023-07-21 6:06 AM
Welcome @Jamer, to the community!
Unfortunately, you have not included a legible photo, but if the marking EV is indeed on the device, it is the SM6T36A. By the way: it is not a Zener, but a TVS = Transient Voltage Suppressor.
If the problem is solved, please mark this thread as answered by selecting Accept as Solution, as also explained here. This will help other users find that answer faster.
Good luck!
/Peter
2023-07-21 6:36 AM
2023-07-21 6:51 AM
Ok, blurred and not very legible, but the package is already the right one. Yes, it is probably the SM6T36A mentioned before.
2023-07-21 6:56 AM
Any idea best place to get one, RS dont have, but maybe FEC
2023-07-21 7:03 AM
Got it....
FEC
Many thanks for your help
2023-07-21 2:23 PM
Great!
If the problem is solved, please mark this thread as answered by selecting Accept as Solution, as also explained here. This will help other users find that answer faster.
Regards
/Peter
We’re moving the ST Community to a new platform to give you a better and more reliable community experience.