2023-07-20 6:51 PM
I drive an AC motor with a triac.
AC is a differential voltage, and the differential voltage of 220VAC is 440VAC.
Then, what size voltage can be used when using the BTA16-600BW model?
220VAC?? Is 380, 440VAC also possible?
2023-07-21 2:14 AM
Please do not confuse the voltage indication on the TRIACs (VDRM = Repetitive peak off-state voltage) with the AC voltage to be controlled. The term differential voltage also comes from a different field and is more commonly used for differential signalling.
Some important terms of the data sheets of TRIACs and SCRs are discussed in AN2703.
Further important basics can be found, for example, in AN4363, section 2.1, where it is explained once again how the VDRM is to be seen in connection with the AC voltage to be switched/controlled.
Summary:
Special attention must be paid to requirements and parameters such as possible overvoltages, motor applications (=inductive loads) and BEMF or even three-phase applications. Therefore, please have a close look at the application notes mentioned so that you can make the right decision.
Hope that helps?
Regards
/Peter
We’re moving the ST Community to a new platform to give you a better and more reliable community experience.