2010-08-28 3:18 AM
I'd like to make the board more useful by desoldering the header plugs on the board and replacing them with sockets I can plug wires directly into.
I've tried using braid and my solder sucker but neither is working effectively. Does anyone have any advice for removing these plugs ? Or am I better off using sockets and headers and so on ?2010-08-28 10:33 AM
Paul,
Try using a little solder on the connections first, The flux in your solder is often better than the flux on cheap desoldering wicks, also your solder will likely have a lower melting point than the boards. then use your solder puller. Personally, I'd leave the board along and use female jumpers, such as those made by Schmartboard. John2010-08-29 6:08 PM
Thanks - I'll look those connectors up :)
2010-09-21 12:50 AM
Paul,
Personally, I unsolder the 2x6 male header that I replaced by females on the copper side.
No trouble for it with a little iron and a pump
In this way, the board can be plug over an extension and i can access to all IO pin.
romainTo give better visibility on the answered topics, please click on Accept as Solution on the reply which solved your issue or answered your question.
We’re moving the ST Community to a new platform to give you a better and more reliable community experience.